(2)| 1/29/2007 10:01 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
[quote user="thuynguyet"]Hi all, I'm trying to count pulses from an encoder using high speed counters on CPU 313C 2DP. Connecting encoder pulse input to the first DI on CPU (I124.0 ???) and calling SFB47 with addr 16#300 (768), channel 0, setting also HW on Count continuously and Count pulse but I still get nothing I've downloaded the example too (for 313C 2PtP), changed the CPU and tried but ... the same things! SW gate and HW gate were also tested but no result! Please help! What'd be wrong? Hello thuynguyet, The first DI on CPU (I124.0) is the pulse input, the second DI (124.1) is the direction and DI (124.2) is the hardware gate. Do you use the Hardware gate? If not you should use only SW gate to start or stop counting. You have put 24Volt on pin 1 and 21 and put ground on pin 20 and 30? I guess you have seen the following manual: http://support.automation.siemens.com/WW/view/en/12429336 You also have seen the examples, you can download from here Best regards, Wizard |
| 1/29/2007 10:41 AM | |
|
Posts: 18 Rating:
|
Thanks very much for early help, Wizard I'll check it all. Do you know if we can test this on Simulation? |
| 1/29/2007 3:38 PM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello thuynguyet, I'm not sure, but I think you cann't simulate. Best regards, Wizard |
| 1/31/2007 2:13 AM | |
|
Posts: 18 Rating:
|
I'm not sure what's wrong, but it's ok now. [:blush:] Any way we can't test it on Sim. Thanks very much, Wizard. |
| 1/31/2007 8:48 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
You're welcome Great it is working now. Best regards, Wizard |
Last edited by: Wizard at: 1/31/2007 8:49 AM |
|
| 5/4/2008 8:39 PM | |
|
Posts: 80 Rating:
|
Hi! I was looking for the examples Wizard mentioned, but i haven't found them yet. Where are those? Thanks pici_c |
| 5/4/2008 9:12 PM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hi, This is the direct link to the example Wizard posted. |
|
Best regards, |
|
Follow us on