Industry Online Support
Technical Forum
4/27/2012 11:59 AM | |
Posts: 57 Rating: (0) |
Hi, Can we use Micro master 440 for high speed winder,unwinder and wire drawing application? |
4/27/2012 1:36 PM | |
Posts: 739 Rating: (55)
|
Hi, it is possible to use a MM440 for winder application. See: http://support.automation.siemens.com/WW/view/en/22095333 MM440 can be used up to 650Hz (fmax = p1082) without encoder. I suggest using a encoder (p0400 – p0494). fmax = 300Hz! To control a encoder with MM440 a Pulse encoder evaluation (oder-no.: 6SE6400-0EN00-0AA0) is needed. Listhandbook See: http://support.automation.siemens.com/WW/view/en/23708204 |
4/30/2012 6:50 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
Hello dear In addition to above link please refer attached document and set parameters accordingly Regards Devesh Vithani AttachmentBasic Winder.pdf (223 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/2/2012 11:03 AM | |
Posts: 57 Rating: (0) |
Hi, Thanks for the post and suggestion. |
Follow us on