(3)| 4/28/2012 7:25 AM | |
|
Posts: 94 Rating:
|
How to calculate the no. of POs? |
| 4/28/2012 9:18 AM | |
|
Joined: 11/4/2011 Last visit: 1/12/2026 Posts: 256 Rating:
|
Have you read Product Support information? How are the licenses for the AS and OS counted as from PCS 7 V7.0? And specify version of your PCS7, because it depends. Cheers. |
This contribution was helpful to
|
|
| 4/29/2012 8:50 AM | |
|
Posts: 559 Rating:
|
Dear Arunraje, What AMAZINGAHMED has told is 100 % true? PO can be calculated by the no of process objects which are going to use in your project. My suggestion is that if you have made I/O list then u must have P&I Diagram then u just calculate the no. of process objects from the P&I Diagram then purchase the license according. |
This contribution was helpful to
|
|
| 4/30/2012 6:34 AM | |
|
Posts: 215 Rating:
|
Hi Arunraje, In addition to above comments, with the help Protime software you can calculate the number of PO's in your project |
| 4/30/2012 10:28 AM | |
|
Posts: 215 Rating:
|
Hi Arunraje, Currently which version of PCS7 you are using? Accordingly i can provide the software |
| 4/30/2012 11:19 AM | |
|
Posts: 94 Rating:
|
PCS7 V7.0 |
| 5/2/2012 1:25 PM | |
|
Posts: 215 Rating:
|
Hi arun raje, I am not able to send you file as its size is more than 3 MB. Can you give me your email ID so i can mail that file to you. |
Follow us on