(0)| 5/4/2012 2:48 PM | |
|
Posts: 4 Rating:
|
Hy everybody. I want to print a trend view graphic. I save data in a csv file. Can anybody tell me how to make it? |
| 5/7/2012 12:26 PM | |
|
Posts: 557 Rating:
|
Hello, Are you using PC runtime or HMI? there is one printfunction available with winCC flex. |
| 5/7/2012 12:42 PM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
In case you have a panel look at this FAQ which could be helpful for you What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)? If you have panel it will be most likely that you print on network printer. Anyway this FAQ should be helpful even if you use local printer. |
|
Best regards, |
|
| 5/7/2012 12:50 PM | |
|
Posts: 1750 Rating:
|
Hello, I don't understand your requirement. Perhaps it might give you some hint for Printing Application. What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels? |
| 5/10/2012 1:27 PM | |
|
Posts: 4 Rating:
|
I make it for PC runtime in WinCC 11 professional |
| 5/10/2012 3:47 PM | |
|
Posts: 3037 Rating:
|
Hello Collin 1, You can log your values in the database in WinCC Professional V11. Then you can export your values from the database to a csv file with the application in the following link. Export of WinCC / CAS Archive Data using the WinCC OLE DB Provider Tweety |
This contribution was helpful to
|
|
| 5/10/2012 3:56 PM | |
|
Posts: 559 Rating:
|
Here is an FAQ on How to archive STRING tags in WinCC Flexible using a script. Archiving STRING tags using a script This can be used for storing values from WinCC Flexible into MS Excel as well |
| 5/14/2012 8:33 AM | |
|
Posts: 4 Rating:
|
I make a full screen graphic, then I print it using printscreen. Anyway, thanks for your replies. |
Follow us on