(0)| 5/11/2012 5:00 PM | |
|
Posts: 947 Rating:
|
1. NTP server and CP must have same subnet. else need a router or change the NTP server address. 2. I believe that the CPU and the CP should have sleduyushie settings - see attachment. 3. i make Hw-config as sample (see attachment.). In the example, may leave traces of the previous project - ignore them. may be this help you Attachmenttune.ZIP (575 Downloads) |
| 5/11/2012 5:39 PM | |
|
Posts: 2348 Rating:
|
Please ensure your NTP-server is recognized by CP as NTP Master. If it's recognized as Reachable synv won't take place. |
| 5/12/2012 4:55 PM | |
|
Posts: 947 Rating:
|
Yello M_Mahallawy in additional: and the MPI-bus here? Forget the MPI. MPI tab is designed to synchronize the time of two processors connected in MPI. Do you have the controller and CP are connected to internal bus. At this time the bus for the CP - the master. Controller - slave. it should be configured. It remains to decide - what to do with the adopted CP time. Because CP is a master - it should bring time forward. Thus, in principle, should work, it is from these it is from these considerations, I sent you a HW-config. Perhaps there is not enough checkbox- set it and check again. I hope - you will understand me, despite my bad English |
Follow us on