(0)| 7/9/2008 10:25 PM | |
|
Posts: 3 Rating:
|
_________________________________------------------------------------ Hello Late, I have a similar problem with two different customers. You mentioned that: "On the properties of the CPU (which one are you using) is on the TAB "Startup" a parameter called "Transfer of parameters to modules [100ms]" which is standard on 100, please place that one on 1000." Ok, I think this could be help, but I have to explain to my customers WHY, how they can calculate this time when they do changes to theirs systems, maybe if they expand the plants. Could you explain me how can I calculate the Monitoring Times (watchdogs) for CPU and I/O modules?? AttachmentCopy of Reporte de Falla caldera 1 CCZ.zip (655 Downloads) |
Follow us on