(1)| 5/16/2012 6:05 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hello. I think you are having Parameter Issue 1) - Regarding Up/Down - Please check Parameters P1000.0 - 1 P1035.0 - 19.D - Raise MOP P1036.0 - 19.E - Lower MOP Note: I assume you are using 1 Command Datasets only 2) - Regarding Value in P759 Check P756 - for selecting whether you are going to use Voltage or Current as AI In P759 - For voltage, max you can select upto 10(V) only and for Ampere, you can select max 20(mA) In addition to this, you have to select DIP swithch accordingly Please refer Parameter List MM440 for more help Regards Devesh Vithani |
Last edited by: Vithani at: 5/16/2012 6:06 AMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 5/16/2012 8:40 PM | |
|
Posts: 621 Rating:
|
Hi Vithani hi i where check the parameter in there P 1035 and 1036 default is there i could not done any thing the application is simple AHU. and in P0756 i selected AI and both dip switches are in on mode. because Scaling 4-20ma. three to 4 times i made factory reseted and also external wiring also checked so what is the other option to solve this problem have you morwe idea plz share with me regards algudkar |
Follow us on