(0)| 5/16/2012 3:34 PM | |
|
Joined: 5/21/2008 Last visit: 12/13/2025 Posts: 93 Rating:
|
pl. have a look http://support.automation.siemens.com/WW/view/en/26437544 sehgal |
| 5/16/2012 3:58 PM | |
|
Joined: 5/12/2006 Last visit: 1/20/2026 Posts: 22829 Rating:
|
Hello, support the PLC Routing? Regards Christoph |
| 5/16/2012 4:17 PM | |
|
Posts: 27 Rating:
|
Yes, I need a manual that discribe how to make routing from Ethernet to Profibus. I' ve only found the opposit. |
| 5/16/2012 4:33 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hi May be following FAQs will help you How is a routing established from one PG via a PROFIBUS interface through a SIMATIC station to SINAMICS G120/G120D frequency inverter via a PROFINET interface? And What should I do if I have set my PG/PC interface to ISO-Industrial Ethernet so I can use Routing with Starter and DriveES to access MICROMASTERS on Profibus from the network port on my PG or PC and I find that the communication doesn't work? Also try searching about routing in Search Field and you will find lot of discussion Regards Devesh |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 5/16/2012 4:49 PM | |
|
Posts: 27 Rating:
|
Thanks you very much This was halpfull Inol |
Follow us on