(0)| 5/30/2012 10:48 AM | |
|
Posts: 1547 Rating:
|
Hello Georgio, i hope i can help a little bit. 1. If you use CP cards you should use Netpro for configuring a connection 2. OC Wizard is only for use with on Board Ethernet interfaces of CPU and much more complex than NetPro. 3. Advanced CP is the biggest cp card you can get in PLC. TCP connection is the same as on other CP443-1 cards. 4. The biggest difference between TCP and ISOonTCP is a problem with variable data length on regular TCP. Refer for this following FAQ: transferring data (with FC5 "AG_SEND" and FC6 "AG_RECV") with variable message lengths via the TCP protocol 5. In Netpro you have to choose the connection Type TCP-Connection. Choose the right ports and call FC5 and FC6 for communication. FC6 will receive only data if you have sent enough data for one job. Try first with some bytes at the parameter RCV in length of your receive block and sent it via hyper terminal. |
Follow us on