(0)| 6/15/2012 2:28 PM | |
|
Posts: 14 Rating:
|
The gsd file. mp277 8" touch [6AV6 643-0CB01-1AX1] |
| 6/15/2012 3:12 PM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
What is your application ? Why do you need it ? It is not available as such. Look here Which GSD files are there for the Profibus DP operator panels? |
|
Best regards, |
|
| 6/15/2012 3:22 PM | |
|
Joined: 9/27/2006 Last visit: 12/31/2025 Posts: 12479 Rating:
|
Hello msarapong; Why? What exactly do you want to do with this gsd file? Make the MP277 a slave to a 3rd-party DP-master? Use the Direct Keys configuration on Profibus-DP? In Siemens's world, an operator panel does not operate as a slave on Profibus-DP; it is a Master Class 2, and has all the rights of any other master on the bus. So the above questions would mark the only reasons you would need the gsd file ofan operator panel;. Look at the following FAQ for more answers, and further links: Which GSD files are there for the Profibus DP operator panels? Hope this helps, Daniel Chartier |
Follow us on