(0)| 7/28/2012 7:49 PM | |
|
Posts: 7 Rating:
|
HELLO, WE HAD AN EXISTING PROJECT IN S7 400 WHICH ONE FC(50) NAMEd lubrication and one for the fc(55) for main motor which will probably INTERLOCKED WITH THE LUBRICATION. SINCE in our mill inlet and outlet oil lubrication has a change over oil filter so that we can make servicing for the back up filter,,but the problem is we cannot changeover the filter when mill is in operation since when binary input adress change from 1 to 0 the main motor totally interlocked. so i tried to create a fault survey with the input of the oil pressure so i can create a delay of a 4 second ,let say memory bit M250.1 in a negate signal and this will be the interlocking of my main motor. in FC(50)LUBRICATION when the input change from 1 to 0 in 4 s elapsed time the M250.1 will change to 1, but in the FC(55)MAIN MOTOR BLOCK, OF THE AST(TOTAL INTERLOCKED) M250.1 REMAINS 0 thats why my motor continue running without interlocked. here attach the snapshot of my project. THANKS,HOPE SOMEONE CAN HELP AttachmentFC WinRAR ZIP archive.zip (106 Downloads) |
| 7/30/2012 7:37 AM | |
|
Joined: 1/3/2006 Last visit: 10/7/2025 Posts: 726 Rating:
|
Use a bit other then M250.1 and see what happens. Check this in PLC.
|
Follow us on