(0)| 8/16/2012 11:52 PM | |
|
Posts: 43 Rating:
|
PLEASE CHECK THE ATTACHMENT |
| 8/19/2012 1:24 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Please mention what problem yuo were facing, and why you have changed CUVC? CUVC doesnt have any LEDs on it. LEDs in attachement is of communication card - one is for Profibus communication - CBP2 and second is for FO - Simolink
Cable is to be made exactly same as in attachement - two 9 Pin Sub D connector - one Male and one Femalerequired as in shown. Male connector is to be connected in Drive - PMU and female connector is to be connected in PC - COM port What is Simatic Box PC you are talking about? If it is PC having COM port, simply connect it
You dont need to enable communication. You only need to set correct baud rate in drive and drive monitor. As far as manual is concerned, best manual is compendium which I guess you already have (attachement is from compendium - I think) Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on