(0)| 11/19/2012 10:40 AM | |
|
Posts: 5 Rating:
|
Dear All, I am using Simocode pro V PN with S71200. I can communicate cyclic with Simocode from S7 1200. But i dont know how to do it Acyclic. Can anyone help me out how to do it. My problem is The Rdrec or Wrrec Function block Record Pointer - DB steps. have refered an sample prrogram in the Support site for Acyclic communication between the PLC and Cu240. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=56749384&caller=view there they have given like this pointer.. H_ReferenceByte0.00 TrueHead: Reference number H_Request IDByte1.01 FalseTrueHead: Request ID: 1=read, 2=write H_AxisByte2.01FalseTrueHead: Allways 1 for SINAMICS G120C H_Number_of_parametersByte3.02FalseTrueHead: Number of parameters to transfer A_1_AttributeByte4.016#10FalseTrueAddress: 16#10 = parameter value A_1_Number_of_indicesByte5.00FalseTrueAddress: Number of elements (0 to 234) A_1_Parameter_numberUInt6.01120FalseTrueAddress: Parameter number A_1_IndexUInt8.00FalseTrueAddress: Index number A_2_AttributeByte10.016#10FalseTrueAddress: 16#10 = parameter value A_2_Number_of_indicesByte11.00FalseTrueAddress: Number of elements (0 to 234) A_2_Parameter_numberUInt12.01121FalseTrueAddress: Parameter number A_2_IndexUInt14.00FalseTrueAddress: Index number how this should be to Simocode. Please help me . i am really held up at project. Anyone has confirgured Profinet Acyclic please help me out for the communication Regards, kaarthikeyan |
Last edited by: kaarthikeyan at: 11/19/2012 1:25 PM |
|
Follow us on