(0)| 12/17/2012 4:30 PM | |
|
Posts: 267 Rating:
|
Hello, I think something is wrong in your program: 1. Please don't use marker (M0.0, MW64, MW80)! You can't be sure if they are used somewhere else. 2. Check your configuration (Input or Input_PER and Output or Output_PER) 3. Is the transition time right? 4. Could it be that you have to invert the controlling direction? 5. Do you use the default PID parameters (Kp=1; Ti=20s)? Do you know this: http://support.automation.siemens.com/WW/view/en/62154322 |
Last edited by: FreakOnALeash at: 12/17/2012 4:32 PM |
|
| 11/27/2017 2:20 PM | |
|
Posts: 8171 Rating:
|
New question published by mugurelgi5 is split to a separate thread with the subject Don't find pid 3_step for step 7 v5.5. Best regards |
Follow us on