(0)| 1/2/2013 12:54 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Anuj; Which bus unit part number are you using to integrate the CP 341s at this time? There are different active busunits that you need to choose from for thedifferent types of S7-300module you plan to use. You can find links to the product support on these bus units here: http://support.automation.siemens.com/WW/view/en/15346950/133200 I believe you should be selecting the 6ES7 195-7HB00-0XA0 model, housing 2x40mm-wide modules. If this is the one you are using and you do not get the 5V power connection, the bus unit could be defective. Hope this helps, Daniel Chartier |
Follow us on