(0)| 1/2/2013 12:47 PM | |
|
Joined: 11/9/2008 Last visit: 1/10/2026 Posts: 414 Rating:
|
Hi All, In my project I want to do Network Redundancy for Wincc. So I have 2 no.of CP1623 in my OS station ,new S7-400H controllers including PROFINET support (S7-400H SYSTEM BUNDLE, CPU 412-5H, 10A, 230V AC : 6ES7 400-0HR01-4AB0)andSCALANCE XB-008 unmanaged8 x 10/100 Mbit/s electrical RJ45 ports (6GK5008-0BA00-1AB2). Please find the attched system configuration for referance and let me know wheter am i able to achive network redundancy for Wincc? Regards, Yogendra G AttachmentSYSTEM CONFIGURATION.pdf (1294 Downloads) |
| 1/3/2013 6:17 AM | |
|
Joined: 11/9/2008 Last visit: 1/10/2026 Posts: 414 Rating:
|
HiDavid, Thanks for your valubale reply. I need some help related configration. This new version CPU 412-5 H PN/DP supporting only TCP/IP not ISO protocol. Kindly help me to configure 2 no.of CP1623 in PC station with TCP/IP netwrok and S7- Fault tolerant connection with PC station in Net-Pro. I am not able to create Fault-tolerant connection. In wincc whether i have to create tag on TCP/IP or Name connection? Please find the atttchement of Hardware configuarion for your referance. Regards, Yogendra G.
AttachmentHW_Configration.pdf (1064 Downloads) |
Last edited by: YogendraG at: 1/3/2013 10:45 AM |
|
| 1/5/2013 1:48 AM | |
|
Joined: 10/7/2005 Last visit: 1/15/2026 Posts: 3054 Rating:
|
Hello YogendraG You need to useISO-on-TCP Fault tolerant connection if you use the PN interface of the H-CPU and prerequisites for this areusage of - CP1623 (which you have) or CP1628 - SIMATIC Net software V8.1.2or later - S7-REDCONNECT Have a look at chapter 14.6.3 of the SIMATIC Fault-tolerant systems S7-400H manual for more on this as well as chapter 4.2 of the just released Configuration Examples for SIMATIC S7-400H with PROFINET(which is generally a good read concerning the different feasibleTopologies for the new N H-CPU's). I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 1/25/2016 10:23 AM | |
|
Posts: 7298 Rating:
|
Hello U_94b3c374-16a3-4d2b-ab04-7760b73b9a18, if you choose "ISO-on-TCP" the S7-REDCONNECT should work with see the manual in the following link: https://support.industry.siemens.com/cs/ww/en/view/90885106
Georg Berghof |
| 8/25/2017 6:06 AM | |
|
Joined: 9/2/2014 Last visit: 5/10/2025 Posts: 10 Rating:
|
Hi All, After going through several links which were dated several years earlier , I just wonder wonder whether Siemens has improved their packages on this. At present, I have a s7-4125H H-CPU station. See attached configuration .( Sorry it is copied from previous post with some edition by my.) I have a WinCC OS station. At present it is equipped with two LAN ports. I am able to connect WINCC OS to s7-CPU via two SCALANCE unmanaged switches to redundant path. But the Connection Driver under the Connections menu allows only one IP address . I want the WINCC communication driver to switch path from 192.168.0.1 ( Master CPU) to 192.168.0.2 ( Standby CPU). whenever there is change in H-CPU status. I have used iFIX ,InTouch or Cytec HMI packages wherein the configuration of the communication drivers allows me to specify a Primary port and Back-up (or secondary) port. This is very standard feature in those software packages . But now with the Siemens Package I do not find it.
Any easier solution or am I missing something to configure in the already standard WINCC package.? Experts , please help. Rgds Kamath RL
AttachmentSYSTEM CONFIGURATION_a.pdf (538 Downloads) |
Last edited by: Kamath RL at: 8/25/2017 6:12:43 AM |
|
Follow us on