4/1/2007 2:04 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Manassas, You may update the hardware catalog, then it is most of the time possible to use new cards. When the new card uses functions from the newer STEP7 version then you will not see the card in the Hardware catalog. See Hardware Support Packages (HSPs)in the pdf you could find which cards are put in the HSP, the CPU you are searching for is in HSP0120. See also How can you update the hardware catalog without direct Internet access? for installing the HSP's intoSTEP7. When you have the opportunity to go directly online, you may use How do I update the STEP 7 module catalog in STEP 7 V5.2 and V5.3? There must also by the new version mentioned which STEP7 version is needed Operating System Updates for CPU 317-2 PN/DPthe text under gives a answer on the question which version you need, for example when you want to use: The above CPU version provides the following new features:
Note on STEP7-related dependencies and upward compatibility: To operate this CPU you require STEP7 V5.3 SP3 or higher. To be able to use the above new functionalities you require STEP7 V5.4 SP1 + HSP0120 or higher. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on