(0)| 1/19/2013 7:33 AM | |
|
Posts: 8 Rating:
|
Hi, I need Profibus Y-Coupler GSD file for 6ES7197-1BL00-OXAO anyone have link .... pls help me to provide a link Thanks Manoj
|
| 1/19/2013 1:56 PM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello Manoj Patel, Siemens , India the Y-Coupler is an integral part of the Y-Linkand if you have an S7 as the DP Master you'll find the Y-Link in the HW catalogue and do not need a GSD file for it. If you have a non S7 DP Master, you need to create a GSD file for the Y-Link and Siemensprovides you with the GSD Tool for this purpose (note that the link refers to the DP/PA Link but the same GSD tool is also used and applicable for the Y-Link). Have a look too at the SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link manual for more info on the Y-Link. I hope this helps |
|
Cheers |
|
| 1/20/2013 9:27 AM | |
|
Posts: 62 Rating:
|
Hi, Thanks a lot... I got it. Bye Manoj |
Follow us on