2/25/2013 7:04 PM | |
Posts: 12 Rating: (0) |
HAMID SIR yes i want to make fb100 in lad .. |
2/25/2013 7:39 PM | |
Posts: 12 Rating: (0) |
i'll try but if u dont mind please give me screen shoot... thank you |
2/25/2013 7:52 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello , What kind of snapshot? You need to read the following manual for a starting point in STEP7,and know how to create an FB. 1-Working with STEP 7 Getting Started As working with TIME data type may cause some problems, use all parameters in floating point (real).Check the attachment to see where you can find instruction for real numbers. Best regards Hamid Hosseini |
2/25/2013 8:39 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello , I have some points to share about your issue: 1- Why do you need to convert FB100 to LAD,if this is your problem.It is possible but you should know STL.If you are not familiar with STL and really good in LAD, try to read descriptions about each STL instruction in online help(by pressing F1) and then select the equivalent in LAD.(Case 1 in attachmnet) 2-If you want to call FB100 in OB35,Just convert it to LAD as I did in case 2 in attachmnet. And finally, you can use FB100 with its interfaces to your program even it is written in German and the worst in STL. Best regards Hamid Hosseini Attachment2_cases.zip (175 Downloads) |
Last edited by: hdhosseini at: 2/25/2013 8:40 PM |
|
Follow us on