(0)| 2/28/2013 8:43 PM | |
|
Posts: 1 Rating:
|
Any idea when will Graph be available? Also anything on CFC? I would love them to make it part of TIA Prof. |
| 3/4/2013 10:04 PM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello muotioj S7-Graph will be part of TIA Portal Step 7 Professional and available for the S7-1500's too. As for CFC I'm afraid to say I don't have the faintest idea if and when it will be available. Seealso page 12 of Siemens S7 TIA Portal brochure wherethe following isstated: SIMATIC STEP 7 V12 provides powerful compilers and programming editors for programming SIMATIC S7 controllers: • The structured text (SCL), ladder logic (LAD), and function block diagram (FBD) languages are available for all controllers. • Statement list (STL) and step sequence programming (GRAPH, SFC) are additionally available for the controller series S7-1500, S7-300, S7-400 and WinAC. |
|
Cheers |
|
| 8/14/2015 2:42 PM | |
|
Posts: 4758 Rating:
|
New question published by Nubber99 is split to a separate thread with the subject When/will CFC be supported on the S1500?. Best regards |
Follow us on