4/25/2007 12:44 PM | |
Posts: 3 Rating:
|
Hi all, I got the ACCON-PG cable which converts 9pin RS232 to 15pin TTY. But the programming port on the AS511 interface module is 25pin. Could anyone please help me wiser with how to adapt 15pin TTY to 25pin on the AS511. I did do some search on the net, knowing that I need to put some power source like +5VDC and 20mA in the circuit but I hope some experts on this forum could make the answer clearer. Thank you with regards, Pattawit, THAILAND pattawit@jpadvance.com |
4/26/2007 11:32 AM | |
Posts: 3 Rating:
|
Thank you for your help Simaticus |
4/26/2007 8:19 PM | |
Posts: 3 Rating:
|
Simaticus, it works !! I jumped around the factory for a couple minutes !! Now I need to focus on modifying some changes in the PLC program of my obsolete Trump TC300W2. Also, I got a fresh document from deltalogic who supplies the ACCON-PG with the adaptor diagram. It works fine as well, so I would like to share it for anyone who faces the same prob as mine. AttachmentACCONCOMKabel_KA_xx.pdf (1371 Downloads) |
4/27/2007 11:47 AM | |
Joined: 1/30/2007 Last visit: 6/3/2022 Posts: 262 Rating:
|
Hi Patt, you 're wellcome. greetings |
8/20/2007 9:30 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi, If I'm not mistaken Best regards, Wizard |
2/7/2019 7:52 AM | |
Posts: 2 Rating:
|
Does anyone have a circuit, pinout cable 6es5734-1bd20? |
Follow us on