(0)| 4/11/2013 12:58 PM | |
|
Joined: 8/25/2006 Last visit: 12/30/2025 Posts: 2221 Rating:
|
Hello. If talk about Simovert MV likehere,first of all be sure that you have source program for Simadyn D created with Step 7, CFC and D7-SYS, as with OmniDrive you can download programs, created with that SW. Anyway to download programs created with CFC to MSxx memory modules you need OmniDrive USB2 LF (LF/SD) or OmniDrive Centronics Professional. If your Simovert MV was programmed with Struc, you need also source program and Parallel Programmer PP1X (or PP1I). If you want to download a parameter backup (.dnl-file) you can't do this with OmniDrive or Parallel Programmer, you need to use DriveMonitor for this.
|
| 4/12/2013 4:02 PM | |
|
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
Hi ! Yes i was speaking about the same in the other FAQ as u mention. Now i have D7 Load setup and also : 0@psw.br3 0@gsw.br3 mv_910.br3 psw.br3 Do i need anything else for doing this job, (beside the hardware of omnidrive pro) |
| 4/13/2013 7:52 AM | |
|
Joined: 8/25/2006 Last visit: 12/30/2025 Posts: 2221 Rating:
|
Hello. D7-Load is old program, and I'm not sure does it support OmniDrive USB (now I can't check this). It will be better to ask Siemens support which version of OmniDrive to use with D7-Load: USB or Centronics. There is also another way to load program, if you have notebook with PCMCIA slot, you can useCardwareas driver for MCxx card and download program by D7-Load.
|
Follow us on