(0)| 5/20/2013 2:38 PM | |
|
Posts: 2 Rating:
|
Hello I've got a project where I have CPU 1214C DC/DC/DC which should control rotating table made by Weiss. That table have a controller called EF2 which is based on Simotion D410-2. Weiss provides special GSDML file (attached). But when I add that controller to my hardware configuration and set my PLC as a IO controller it end with error during config downloading"Loading the hardware configuration failed(00200 2 0)" Thanks in advance for any help! Best regards, Marcin R.
AttachmentGSDML_WEISS_EF2_PN01.zip (765 Downloads) |
Last edited by: Marcin Rumanek at: 5/20/2013 3:03 PMLast edited by: Marcin Rumanek at: 5/20/2013 2:50 PM |
|
| 5/21/2013 7:17 AM | |
|
Posts: 2 Rating:
|
It's v3.0 (6ES7 214-1AG31-0XB0). Screenshot of I/O and network attached. |
Follow us on