Industry Online Support
Technical Forum
6/13/2013 5:47 AM | |
Posts: 4 Rating: (0) |
Hello Everyone, I have a hardware downloadproblem with Simatic Manager. In the hardware I have many I/O modules and also two Simotion CPUs. One of them is Simotion D445 and the other is Simotion D425. I upload the program by opening a blank project and selecting Upload Station to PG from the CPU 424-2DP and then I press on the download button without no change but it gives an error "The slave C2xx/P3xx/D4xx ISlave in the DP master system Profibus DP Machine: DP master system (1) does not contain an assignment of the logical master/slave addresses." If I remove the station boxes of these two simotion CPU the error does not occur. You can see the screenshots from the attachemets. What can I do to solve this issue? What is the problem. The configuration inside the CPU is not correct? How can I add an assignment of logical master/slave addresses? AttachmentHardware.zip (131 Downloads) |
6/17/2013 9:54 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Hardware Download Problem Best regards O_Moderator |
Follow us on