(5)| 5/23/2007 5:15 PM | |
|
Posts: 10 Rating:
|
Helmut I copied the folder from the CD ( <cd drive>windows/tools/applications) to my hard-drive C: then located the logocomfort.exe - rightclick - properties - compatibity - Windows XP or earlier. Also add shortcut to desktop. (see attachment) Thanks Michael The problems with vista and Logo Soft is that the installation program that SoftComfort uses (InstallAnyWhere) is not Vista compatable. They are a lot of installation programs that have worked for years on Windows 98/Me/2000/XP/2003 that just will not work on Vista. The only one that I have found to work is *InstallShield*, which is the most common one, so why Siemens did not use it on Softcomfort I can not work out, they did on the other Softwares (Step7-Lite, Micro-win etc) AttachmentLogo Vista.pdf (1145 Downloads) |
Last edited by: STOKIE at: 24.05.2007 09:37attached a correted pdf of installation Last edited by: STOKIE at: 24.05.2007 09:31Last edited by: STOKIE at: 24.05.2007 09:30added a pdf explaining how to install Logo Soft 5 on to a VISTA machine. |
|
| 7/26/2008 7:38 AM | |
|
Posts: 95 Rating:
|
This link will really help too: http://support.automation.siemens.com/WW/view/en/22113982 |
| 9/1/2008 2:49 PM | |
|
Joined: 10/3/2007 Last visit: 1/15/2026 Posts: 3 Rating:
|
Thanx for the help guys |
Follow us on