(0)| 7/12/2013 12:24 PM | |
|
Joined: 9/27/2006 Last visit: 12/31/2025 Posts: 12479 Rating:
|
Hello Adrian; To add to Hamid's post, each DO module has a different parameter set, some accept a substitute output value, others do not, as you can see in the attachement below, taken from this manual: SIMATIC S7-300 S7-300 Module data So we need to know the exact part number of your DO module, or you can look the information up by yourself in the manual. The substitute value, if available, is set through the module parameters, in the HWConfig editor. There are no OBs that cover this functionality. Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
| 7/12/2013 12:25 PM | |
|
Posts: 20 Rating:
|
Okay, I think I am getting it now. CPU: 315-2 PN/DP 6ES7 315-2EH14-0AB0 DO: 16x24vdc 6ES7 322-1BH01-0AA0 |
| 7/12/2013 12:46 PM | |
|
Posts: 95 Rating:
|
hi it is depend on hardware that use some output hardware have this options to set output in case of plc stop this options are that you can adjust output in last value or you adjust output. Attachmentp1.zip (751 Downloads) |
Follow us on