7/13/2013 6:19 PM | |
Posts: 378 Rating: (73) |
Hello Raja soundar,
Regards |
7/13/2013 6:26 PM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating: (1360) |
Hello, Similar diskussion previously in the following link and coming with a fantastic working solution: WINCC Client Graphich screen updating slow
Just an idea, hope helps Hamid Hosseini |
This contribution was helpful to1 thankful Users |
7/15/2013 10:45 AM | |
Posts: 21 Rating: (0) |
Hidesmul24, I have attached my network architecture here. when I run Wincc V7 RT in 2 servers(Redundant), both the servers are really quick in updating PLC values. Then if I activate runtime in any two clients, then also it is working fine. If I activate runtime in third client, the scada is taking 25sec to update tag values from PLC. Also the server (SERVER A) which the three clients are pointing to is slow but the standby server (SERVER B) is fast. If i make three clients point to SERVER B then SERVER B is slow and SERVER A is fast. we called siemens network expert and he told there is no problem in the network, the problem is at application level. Any clue where I have to look into. Regards, Govind.
|
7/15/2013 10:56 AM | |
Posts: 21 Rating: (0) |
I increased the virtual memory. but still its slow. |
7/15/2013 11:31 AM | |
Joined: 10/3/2010 Last visit: 6/25/2024 Posts: 1556 Rating: (190) |
Raja, iIt's hard to tell what is wrong, cause can be several things: scripts waiting for each other, update cycles used on your pictures,... Please check your log-files, usually under "C:\Program Files\Siemens\WinCC\diagnose"...especially the ones related to your communication(s). Check these logs for entries around the time that your problem(s) start. |
B r g d s , |
|
7/15/2013 12:43 PM | |
Joined: 10/3/2010 Last visit: 6/25/2024 Posts: 1556 Rating: (190) |
usually there are several log files in that folder? Check the one whose names is related to your communication channel, for example "SIMATIC_S7_PROTOCOL_SUITE_01.LOG" |
B r g d s , |
|
7/15/2013 8:18 PM | |
Posts: 559 Rating: (87) |
Have u defined the tag update upon picture cycle? |
Follow us on