Industry Online Support
Technical Forum
7/20/2013 8:01 PM | |
Posts: 7 Rating: (0) |
@Jaapie: could you please kindly provide the script for sending sms messages? |
Last edited by: O_Moderator at: 7/23/2013 9:46 AMnew subject after splitting from /tf/WW/en/Posts/25481#top Last edited by: ceca at: 7/20/2013 8:02 PM |
|
7/23/2013 10:27 AM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Hi Ceca, So I made you a nice package . 1- gmsgfunc script to show you a little bit how it works (not tested because it's from a big specific project and all "secret" stuff is deleted). 2- OPRCL32 is the dll you need (but you fist need to install the diafaan software). You can call Diafaan, no problem they are very helpfull. 3-Oproep_WinCC (Oproep = dutch for "Call") is a .h file you need to place in the apbib directory of WinCC (where all .h files are located). Then you need some testingI think, because it will not work right away because I changed the script to delete the specific project functions. I used it for sending to "pagers" so you also need to change that in the script I send, but it will work for sure. Don't hesitate to call Diafaan, again they are very helpfull. I'm offline for a few weeks so no more help from my side, sorry. Good luck, Jaap AttachmentSMS.zip (193 Downloads) |
Last edited by: O_Moderator at: 7/23/2013 11:30 AMattachment reattached |
|
7/23/2013 6:55 PM | |
Posts: 7 Rating: (0) |
Thank you a lot anyway and have a nice vacation! |
11/13/2014 10:25 AM | |
Posts: 10 Rating: (1) |
Could not extract files with winrar, but with 7-zip it worked. |
Follow us on