(0)| 9/8/2013 8:08 AM | |
|
Posts: 19 Rating:
|
Dears All, I am proposing one system.There are two remote stations. Each with S7 400H with ET200M Redundant Bundle & CP 343-1 with Open Modbus/TCP Blocks. These RTU's needs to remotely communicates via Modbus TCP/IP to GSM Gateway with the central SCADA WinCC 7.0 I am using CP 343-1 with Open Modbus/TCP Blocks only for communicating to WinCC SCADAthrough Modbus TCP/IP to GSM Gateway. The Client requirement is to use GSM Network and Modbus TCP/IP. This is relative small system so I am not going on telecontrol system. Both RTU's acts as Server ( Slaves) and WinCC SCADA as Client (Master), which collect data and send commands to RTUs. Can you kindly suggest me , This is a feasible solution & it works. Also shall I need any additional software packages. Thanks in advance. AttachmentProposed Configuration.pdf (238 Downloads) |
Last edited by: M Saad Khulsai at: 9/9/2013 7:56 AM |
|
| 9/9/2013 12:17 PM | |
|
Posts: 3093 Rating:
|
Hello Saad, you can't run a CP343-1 with an IM153-2. Regards, Kaulquappe |
Follow us on