(1)| 6/10/2007 11:58 PM | |
|
Joined: 6/2/2007 Last visit: 11/17/2025 Posts: 9 Rating:
|
Hi, the device is a Datalogic DLC 6065 barcode reader (without button) usingserial port via RS 232 protocol (9600, 8-bit, No Parity, TRUE). Attached to this msg you can find one ofmy test....(some segments has been wrote to the aim to compare the readed barcode with a reference code (in this case the number"4") in order to abilitate a physic output...... (Q0.0) Concerning PLC, unfortunately I have S7 224 and 214 only. If you could help me I will be very thankful. Thanks for the attention, Guido Attachmentbarcode_test.zip (475 Downloads) |
Follow us on