(0)| 10/16/2013 3:45 PM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, There are no commands in S7 that can replace the LIR and TIR. The From S5 to S7 Converter Manual States: In general, not all the parts of a program can be converted. Considering the following points will help you decide whether to convert your S5 program or to recreate it in S7. .. Absolute addresses cannot be addressed in S7. The corresponding instructions (such as LIR, TIR, etc.) are not converted. If a program frequently works with absolute addresses, it is a good idea to rewrite these parts of the program or, if necessary, the entire program. If you use the keywords lir or tir in the search field, it will lead you to some explanations how to convert it . Regards, Marcjan |
|
Problem solved? |
|
Follow us on