(0)| 11/17/2013 8:36 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Setting range for P640 is from 10% to 400% so ofcourse you can set it to 50% But remember, it will only restrict current to that level and for that, it will reduce frequency if current tries to go high If you want to make it trip immidiate, you need to set external trippings - for that refer here |
Last edited by: Vithani at: 11/17/2013 8:37 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on