2/27/2015 8:33 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello; Sorry, but the message you sent was garbled; I will try to answer as best I can Under the circumstances. The best place to locate information on Wago modules is the Wago.com website. Searching for the 750-333 Profibus-DP coupler, you will have been presented these documents:
Wago 750-333 configuration as slave in Step 7: Application Note http://www.wago.com/wagoweb/documentation/app_note/a1008/a100800e.pdf Wago 740-333 GSD file: GSD files for PROFIBUS with installation program / 750 Start with the installation of the gsd file, as shown in the application note.The gsd file is an executable, simply run it and it will install the required files (I do not believe you need the S5 gsd files) directly in the correct directory of Step 7. Then select and configure the IO modules on your Wago coupler for insertion in the Profibus configuration. Follow the example in the application note. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/27/2015 8:35:24 PM |
|
2/28/2015 10:42 AM | |
Joined: 2/11/2015 Last visit: 1/15/2024 Posts: 14 Rating: (0) |
Hallo Thanks.i am gonna check that Greetings |
Follow us on