6/27/2014 1:47 PM | |
Joined: 6/8/2013 Last visit: 8/5/2024 Posts: 188 Rating: (1) |
thank you Mr.kaulquappe |
3/3/2015 8:27 PM | |
Joined: 12/29/2014 Last visit: 8/27/2024 Posts: 16 Rating: (0) |
Kaulquappe, Thank you for your response been of great use to solve my doubts about the FB108 block. The network is not reduntante. I have other questions regarding the correct way to use MODBUSCP blocks. In my application I wish my CP to communicate with 4 servers and a client, each on a different port CP. The settings have NetPro the list, there have no doubt, but with regard to the correct way to call the blocks is where I have serious doubts. And I would answer me or confirm the following questions if you do not mind: 1. The OB100 used to initialize Blocks "MODBUSCP". So in this OB I must put 5 "MODBUSCP" each parameterized according to the manual. 2. There should only be a block "MODBUSCP" for each cyclic OB. 3. What is the correct or most efficient way to work several "MODBUSCP" since these blocks are memory intensive work. See chart, Thank You AttachmentMODBUSCP.pdf (593 Downloads) |
Last edited by: JoelHuaman at: 3/3/2015 8:30:09 PMLast edited by: JoelHuaman at: 3/3/2015 8:34:05 PM |
|
Follow us on