3/6/2015 4:55 PM | |
Posts: 74 Rating: (0) |
I cant get my project smaller than 3000 bytes is it possible to just upload my OB35 and my OB1? |
3/9/2015 11:10 AM | |
Posts: 74 Rating: (0) |
Hi, I have uploaded a simplier version of my project in contsin my OB1 OB35 and the DBs. What I wanting to do is to fill a tank to a setpoint using the PID block. The actuator to be controlled is a pump with a varible motor speed and a ultrasonic level sensor is used for the level control. regards
Jimbo AttachmentExample1.zip (199 Downloads) |
3/10/2015 5:32 PM | |
Posts: 74 Rating: (0) |
Hi Thank you, would it possible to provide the code in FBD Regards |
3/10/2015 5:46 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
It is easy it for it by yourself.Copy each section of codes and stroke key combinations "CTRL+3" and "CTRL+2"
|
3/11/2015 4:41 PM | |
Posts: 74 Rating: (0) |
Hi, Is this placed in OB100 or in OB1? |
Follow us on