4/13/2015 10:27 AM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating: (175)
|
Hello Reymond,
If you have 5 load cells, you can use two pieces of aluminium housing junction boxes with the order number: 7MH4710-1BA.
Into the attached manual you can find into the chapter 1.1 a sketch with two junction boxes.
You have only to connect all load cells in parallel, that means: connect all EXC+ together, all EXC- together, … and so on.
Best regards
Siwarexi
AttachmentBA_SIWAREX_JB_ALU-Gehaeuse_en.pdf (153 Downloads) |
Follow us on