3/27/2015 9:21 PM | |
Joined: 3/4/2011 Last visit: 11/1/2022 Posts: 78 Rating: (4) |
Thanks for the reply Helmut. I have checked, re-checked and checked again. Everything works perfect in Sim and as you say drag and drop makes it very easy. I have included the program for your entertainment. I1 sets the low level and turns on Q1 I3 is the pulse counter After a 3 second delay Q2 turns on and the pulses are counted into a second register. Q3 should output to NI1 on the second LOGO Q4 should output to NI6 on the second LOGO AttachmentNet_IO.zip (169 Downloads) |
Follow us on