11/7/2014 8:53 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, Have you seen this link: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
11/13/2014 10:34 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, Perhaps the following link might help: how can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? (it is important to change the name of the panel, it must not be standard) Best regards, Wizard |
4/21/2015 9:37 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Kris, Have a look: Which connector cables are available for connecting to SIMATIC Panels? |
Follow us on