4/14/2015 5:45 PM | |
Posts: 93 Rating: (0) |
Hi expert, i am used the simatic field pg part number( 6ES7 712-OAA01-OBE4) for programming. In MPI PC ADAPTER connect to the simatic field PG all block not going to run mode,but i connect the ethernet cable all block going to run mode. i cross check with mpi pc adapter cable connect to laptop all block going to run mode. IN PG/PC interface i select PC ADAPTER AUTO,when click online monitoring the alarm popup communication link demaged. one more information last week some issue in PG.So our team done the OS reinstalled that PG,that may be problem for this issue? Now we are using ethernet mode for online monitoring.But also i need MPI PC ADAPTER mode also. Pls guide me to solve the issue. Advance thanks&Regards, Suryamuni.
Attachmentonline issue.pptx (105 Downloads) |
4/17/2015 10:04 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello Please give MLFB number of cable you are using? (6ES7.....) And you are using a Field PG? Best regards, Wizard |
4/17/2015 7:38 PM | |
Posts: 93 Rating: (0) |
Hi Wizard, Thanks for your reply. PC-ADAPTER CABLE PART NUMBER : 6ES7 972-OCB20-OXAO FILED PG PART NUMBER : 6ES7 712-OAAO1-OBE4 Regards, Suryamuni |
Follow us on