4/21/2015 9:07 AM | |
Posts: 457 Rating: (46) |
Hello rollex, there are two questions regarding your post: 1. do you want to show data which is stored in SQL-database? Then you must use Datamonitor. No other way possible. 2. if you want to show only actual tags then you can open a csv-file by script and write tags in this file manually. Regarding this feature, please make a search within Siemens-support sites. There a lot of examples, here is one: https://support.industry.siemens.com/tf/ww/en/posts/58217/ Best regards Georg |
This contribution was helpful to1 thankful Users |
4/23/2015 9:05 AM | |
Posts: 457 Rating: (46) |
Hello, WinCC 7.0 SP4 provides a secured database for tag logging. You cannot access DB by SQl or any other commands directly. Only solution for data export is a Siemens Add-On-Tool. There are some addons like PM-Open-Export, Industrial Databridge (http://w3.siemens.com/mcms/human-machine-interface/en/visualization-software/scada/wincc-options/wincc-industrial-data-bridge/pages/default.aspx) or Process Historian. I think Process Historian will be the solution. Georg
|
Follow us on