4/21/2015 8:39 PM | |
Posts: 11 Rating: (0) |
New Question related to TCP communication. Is it possible to use an S7-1212 to send SCPI commands and receive data directly to/from an oscilloscope that is connected via an ethernet cable to the same network as the PLC. As both support TCP communication I was hoping this would be possible. I have tried using the TCON function, but so far it won't connect. The PLC and scope are connected via an ethernet switch. Perhaps I need some other component to enable the PLC to recognise the scope?
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/22/2015 10:12:39 AMNew subject after splitting |
|
Follow us on