4/30/2015 4:53 PM | |
Joined: 4/28/2015 Last visit: 9/26/2022 Posts: 1 Rating: (0) |
There is an ongoing issue at Wagstaff on control circuits in Class 14 coils with what seems to be excessive high temperatures. Please take a look at the attached photos and advise response for CED Spokane who is the local supplier of these devices through the maintenance contractor Rainbow Electric.
Same problem with class 87 pump panel when wired for 240V excessive heating and in one case when the HOA is in the off position,
Seems to be a reoccurring problem with dual voltage rated coils. I send samples to replace
please advise resolutions, or ideas that will resolve this on going problem.
Mike Bjur
AttachmentEF -1.pdf (957 Downloads) |
Last edited by: Min_Moderator at: 4/30/2015 5:33:56 PMContact data deleted |
|
Follow us on