5/26/2015 4:16 PM | |
Posts: 16 Rating: (0) |
Good day Mr experts / users. The operation panel displays the image with a 180-degree turn, I know how to solve this problem. |
5/26/2015 9:52 PM | |
Posts: 16 Rating: (0) |
WinCC Flexible 2008 SP2 K1.3.2.0_1.58.0.1 OP 277 6" |
5/28/2015 9:15 AM | |
Joined: 8/3/2009 Last visit: 5/6/2024 Posts: 12884 Rating: (1645) |
Hello yv@n I know this behaviour. The display is mirrored. this looks curious. The Reasen could be: - Software defect: the Operating System or the display drivers are corrupted Here you can do an Reset to Factory Settings with this FAQ: https://support.industry.siemens.com/cs/ww/en/view/19701610 (use the Prosave manual) (perfor a Backup first to get save: https://support.industry.siemens.com/cs/ww/en/view/28928853 ) - Hardware defect: if the Reset to factory settings do not work or the behaviour is still the same, your hardware is probably defect, so you have to send it to repair: https://support.industry.siemens.com/cs/ww/en/view/22639376 wish you the best Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
5/28/2015 7:53 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello yv@n, Perhaps might help you??? |
Follow us on