6/30/2015 6:33 AM | |
Joined: 10/21/2013 Last visit: 9/19/2024 Posts: 417 Rating: (28) |
Hi Girish, you cannot use wincc flexible 2008 sp2 rt directly in windows 7 . you need to upgrade to sp3.you do not need any licence for upgrading but you need Upgrade CD. pls find the link for more info. https://support.industry.siemens.com/cs/document/57267466?dti=0&lc=en-WW |
This contribution was helpful to1 thankful Users |
6/30/2015 10:36 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1732) |
Hello girish bodhale Yes its Right you have to use the same Version of WinCC flexible on your Runtime System and on your Engineering system Yo you have to do an upgrade to WInCC flexible 2008 Sp3. You can use the downloadlink fo the Trial software, its the whole Software and can be used with a valid WinCC flexible License https://support.industry.siemens.com/cs/ww/en/view/100777999 You should also use the lateste Updates: https://support.industry.siemens.com/cs/ww/en/view/58860033 After the Upgrade open your Project in WinCC flexible again and convert it into SP3 Project. Now do a download to your new Runtime System and you can run your Project. Have a nice Day Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on