5/19/2015 12:48 PM | |
Posts: 45 Rating: (0) |
hi ! how to set groupo_nro in HMI tag
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/19/2015 4:06:38 PMNew subject after splitting |
|
5/20/2015 10:08 AM | |
Posts: 82 Rating: (3) |
Hi mamadou13. I think your question concerns to the alarmgroup. The alarmgroup you do not change in the HMI Tag but in the discrete alarm.
Regards, JRB28. |
7/2/2015 3:25 PM | |
Joined: 4/26/2012 Last visit: 4/19/2024 Posts: 1517 Rating: (158) |
you have to use the load event, the "Logon" function. attached I made an example. Description Logs on the current user on the HMI device. Use in the function list Logon (Password, User name) Use in user-defined functions Logon (Password, User_name) Can be used if the configured device supports user-defined functions. For additional information, refer to "Device dependency". Parameter Password The tag from which the password for the user logging on is read. If the user is logged on, the password in the tag is deleted. User name The tag from which the user name for the user logging on is read. boa sorte. Attachmentzip.zip (106 Downloads) |
Last edited by: rdoliveira at: 7/2/2015 3:27:45 PM"Always make a backup before and check the best time before testing." |
|
Follow us on