7/4/2015 1:49 PM | |
Joined: 11/29/2011 Last visit: 4/19/2024 Posts: 1349 Rating: (229) |
Hi, Look at SIMATIC S7-300 CPU 31xC Technological Functions manual under chapter"5.7 Description of the Pulse Width Modulation Functions". I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
7/4/2015 8:05 PM | |
Posts: 7 Rating: (0) |
i want to ask what is the use of the hardware gate and what is a filter frequency ?? |
7/4/2015 10:17 PM | |
Joined: 11/29/2011 Last visit: 4/19/2024 Posts: 1349 Rating: (229) |
Hi, Hardware Gate: It is an option you can use to control the PWM function. SIMATIC S7-300 CPU 31xC Technological Functions chapter "5.7.5 Gate Function of Pulse Width Modulation". You can read: "A hardware gate (HW Gate). You can assign the hardware gate in the parameter You can check the assigned terminal numbers under chapter "5.2.2 Pin Assignment"/Pin assignment CPU 313C (connector X2) or CPU 313C-2 DP, PtP (connector X1). Note: The relation of SW/HW gate is described in the chapter 5.7.5. Filter frequency: The HW gate is a DI in some extent, so its signal is filtered within the card. Similar question discussed in Filter on Digital Inputs. I hope I could help! |
Last edited by: MicroMan at: 7/4/2015 11:09:26 PM- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
7/5/2015 12:46 PM | |
Posts: 7 Rating: (0) |
can i use a counter to count the pulses generated by the function SFB 49 because i tried but it fails i do not know what is the problem?? |
Follow us on