3/15/2015 1:22 PM | |
Joined: 12/2/2008 Last visit: 3/4/2024 Posts: 25 Rating: (1) |
Windows 7 SP1 32bit Application S7-PLCSIM v13 SP1 crashes on creating project (Siemens.Simatic.PlcSim.VplcHost.exe) Without SP1 - appication works fine Without SP1 there is set of registry keys in [HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\SINEC\LogDevices\PLCSIM S7-1200/S7-1500(TCP/IP)] When installing SP1 - all keys are eraised in that location I tried to add that keys by mysefl, but got tia portal chashes at project opening Does anybody knows how to fix s7-plcsim v13 sp1 ?
|
Last edited by: fary312 at: 3/15/2015 1:29:43 PMLast edited by: Min_Moderator at: 3/16/2015 2:15:17 PMNew subject after splitting |
|
6/5/2015 11:26 AM | |
Joined: 4/28/2015 Last visit: 1/4/2024 Posts: 2 Rating: (5) |
Windows 7 SP1 32bit Application S7-PLCSIM v13 SP1 crashes on creating project Solution: Repair with the patch (delivered by Siemens Hotline 2015-06-04) You can download the file here: (or attached) Here is a registry which stops the crashes with the TIA Portal V13. But it is only for 32 bit Windows. AttachmentRepair_PLCSIM_V13_SP1_32bit.zip (1313 Downloads) |
7/5/2015 2:37 AM | |
Joined: 7/1/2015 Last visit: 6/6/2020 Posts: 2 Rating: (0) |
|
7/5/2015 2:39 AM | |
Joined: 7/1/2015 Last visit: 6/6/2020 Posts: 2 Rating: (0) |
|
9/23/2015 3:22 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by APS_84 is split to a separate thread with the subject TIA simulator V13 SP1, system crashed. Best regards |
7/25/2016 10:07 AM | |
Posts: 6 Rating: (4) |
Updates for PLCSIM V13 SP1After installed it is ok. https://support.industry.siemens.com/cs/document/109477180/updates-for-plcsim-v13-sp1?dti=0&lc=en-DE |
Follow us on