1/16/2014 4:47 PM | |
Joined: 4/25/2009 Last visit: 4/19/2024 Posts: 20 Rating: (2) |
Hi I didn't know in step7 V5.5 I don't need to install USB PC adaptor's driver. so I installed it and this is the result:
I'm using Windows7 64 bit !
AttachmentPgPcInt.zip (1324 Downloads) |
Last edited by: GrasserF at: 1/17/2014 10:49 AMnew subject after splitting from /tf/WW/en/Posts/61586 Last edited by: 30A at: 1/16/2014 5:02 PM-------------------------------------------- |
|
1/28/2014 12:28 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, I recommend to delete the driver in the device manager of Windows 7 and start the PC again. After and during the new start of Windows 7 the driver of the PC adapter will be new installed and then it should be possible to use it. See also the informations of the FAQ (link): http://support.automation.siemens.com/WW/view/en/37855422 With best regards |
4/9/2014 1:46 PM | |
Joined: 4/8/2007 Last visit: 4/25/2024 Posts: 1 Rating: (0) |
hi guys I'm using Windows 7 x64 too and I have the same problem. regards |
4/24/2014 10:49 PM | |
Posts: 1 Rating: (0) |
Yes, this problem I have too Win7/64bit, Step7 v5.5, USB-MPI adapter. |
4/29/2014 1:29 PM | |
Joined: 8/25/2005 Last visit: 3/21/2024 Posts: 1161 Rating: (110) |
Hello, I have seen the post published by GrasserF: Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5Is this the solution you are looking for? Good luck Sabine |
Follow us on