7/27/2015 8:50 PM | |
Posts: 2 Rating: (0) |
Hi. I have an application using S7-400 CPU 416 with CP443 and some drives (MM440, Sinamics, Masterdrives) on Profibus. Almost all drives could be routed (via ethernet >> profibus) but I'm having problems with the only two Sinamics G120 CU240E-2DP V4.5 6SL3244-0BB12-1PA0. Only these two Sinamics G120 could not be routed with Starter V4.4. The GSD and CU240E-2DP are with the same version 4.5. It's possible to see some screenshots attached of the HW Config and Starter configuration. Please, any idea about this problem ??
best regards, XKTO
AttachmentCU240E2DP.zip (73 Downloads) |
Last edited by: XKTO at: 7/27/2015 8:53:21 PM |
|
7/28/2015 6:29 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello,
which FW Versions you use for the S7-400 and the CP443? Check if you have the right versions for Routing: https://support.industry.siemens.com/cs/ww/en/view/50037141 Christoph |
Last edited by: ChristophD at: 7/28/2015 6:30:08 AM |
|
7/29/2015 8:13 PM | |
Posts: 2 Rating: (0) |
Hi ChristophD. Thanks for the quick help. So, the problem with routing is the CPU 416-2 DP version (V3.1).
best regards.
|
Follow us on