7/17/2015 11:18 AM | |
Posts: 70 Rating: (1) |
Hi, I have a sensor that gives me a signal 0-10V, according to the pressure (0-1 meter) and I do a Norm_X function and after I do an Scale_X function. Thanks |
7/22/2015 8:26 AM | |
Joined: 5/9/2011 Last visit: 3/21/2024 Posts: 70 Rating: (5) |
Not sure if this will work with a real analog signal but might be worth a try. Check out the small user program in Step7 attached where MW130 is the level input, instead of subracting from the level you can add 5 every time when you start at zero level and compare the difference. Then you can use M50.1 to trigger your fluid injection.AttachmentLEVEL_2.pdf (345 Downloads) |
8/1/2015 8:23 AM | |
Joined: 5/9/2011 Last visit: 3/21/2024 Posts: 70 Rating: (5) |
Hi Bruno, check out the revised program in TIA portal which is attached as pdf. Change the compare block to a greater than block and use the move function to reset the count to 0 when the level drops below 5. I am not sure however if the pressure sensor for the level is the correct solution for such a small tank, you might need to look at other level sensors to give a more accurate and updated response to the fast changes in the level. Regards AttachmentTANK_2.pdf (293 Downloads) |
Follow us on